DIN#.STATE
Description
Reads the state of one digital input according to the number identified in the command.
Examples
Code
--> DIN1.STATE 1
Context
For more information see Digital Inputs and Outputs.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read Only |
Units | N/A |
Range | 0 to 1 |
Default Value | N/A |
Data Type | Integer |
See Also | |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.